Is any console log output from UART if I download MAC 2006 FSCI 115200 KW41 ASP_RadioTest.srec into FRDM-KW41Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is any console log output from UART if I download MAC 2006 FSCI 115200 KW41 ASP_RadioTest.srec into FRDM-KW41Z

1,819 Views
Danube
Contributor IV

Hi Sir,

I can't see any console log from OPENSDA debug port if I download MAC 2006 FSCI 115200 KW41 ASP_RadioTest.srec into FRDM-KW41Z.

1 Reply

1,440 Views
karel_povalac
NXP Employee
NXP Employee

Hello Danube‌,

I tried to compile and load the MAC_FSCI_app for the FRDM-KW41Z. I sent the console commands through the NXP Test Tool 12. The board responded on the console. Please try to use it (load the MAC2006_g command set). The Test Tool will also decode particular commands.

Karel