Integration of LVGL with KW45B41Z-EVK Using LCD-PAR-S035

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integration of LVGL with KW45B41Z-EVK Using LCD-PAR-S035

411 Views
Pavankumar1
Contributor III

Hi sir,

I am working on the KW45B41Z-EVK board and would like to integrate LVGL with the LCD-PAR-S035 display. I need clarification on the feasibility of this integration.

Could you please confirm whether LVGL can be successfully integrated with this display on the KW45B41Z-EVK? Additionally, if integration is possible, are there any reference drivers or examples available to assist with the implementation?

Any guidance or documentation regarding this setup would be highly appreciated.

Looking forward to your response.

Best Regards,
Pavanakumar A G

0 Kudos
Reply
1 Reply

380 Views
luis_maravilla
NXP Employee
NXP Employee

Dear Mr Pavanakumar

NXP has an example that integrate LVGL with the LCD-PAR-S035 display in FRDM-MCXW71

Here is a link in the Application code hub for NXP

https://mcuxpresso.nxp.com/appcodehub?search=dm-mcxw71-driving-lcd-wireless-uart

And the link for the same application in NXP Github for downloading the files

nxp-appcodehub/dm-mcxw71-driving-lcd-wireless-uart: allows the user to interact with the device thro...

 

This has the documentation / DRIVERS / code that you will need to implement in the KW45B41Z-EVK board.

 

Best Regards

Luis

0 Kudos
Reply