已解决! 转到解答。
Hi David,
I'm sorry, my misunderstanding. I thought do you want to design the gateway IoT with an Ethernet MCU.
Is this possible to achieve ? and is there any example or application note supporting this?
What are the challenges and considerations I would need?
You can add another Zigbee product. As you know, the ZigBee protocol is a standard and all the products should be compatibles, that is the reason for Zigbee Alliance.
Also, you have to be sure that the stack is compatible, for example,
The JN-AN-1189 is a simple demonstration from ZigBee Home Automation Profile Specification version 1.2.2, so, the external device has to be compatible this version and the stack that you are working on(ZHA, ZLL, ZB3...).
Hope it helps.
Regards,
Mario
Hi David,
You are working with the Control Bridge for the Zigbee devices. I recommended the LCP 54618. LPC546XX|NXP
Download the SDK https://mcuxpresso.nxp.com/en/dashboard,and take a look at the HTTP server that we provide.
As you know the MCU supports Ethernet MAC with MII/RMII interface with Audio Video Bridging (AVB) support and dedicated DMA controller.
Please let me know if the information was useful.
Regards,
Mario
Hi mario_castaneda ,
Thanks for your reply.
Is there a problem with JN516x based modules ?
The job I want to do is to be able to communicate wirelessly with other zigbee devices using zigbee protocol.
I'm trying to achieve interoperability for my hub to be able to integrate other different zigbee products with it.
Is this possible to achieve ? and is there any example or application note supporting this ?
What are the challenges and considerations I would need ?
Thanks.
Hi David,
I'm sorry, my misunderstanding. I thought do you want to design the gateway IoT with an Ethernet MCU.
Is this possible to achieve ? and is there any example or application note supporting this?
What are the challenges and considerations I would need?
You can add another Zigbee product. As you know, the ZigBee protocol is a standard and all the products should be compatibles, that is the reason for Zigbee Alliance.
Also, you have to be sure that the stack is compatible, for example,
The JN-AN-1189 is a simple demonstration from ZigBee Home Automation Profile Specification version 1.2.2, so, the external device has to be compatible this version and the stack that you are working on(ZHA, ZLL, ZB3...).
Hope it helps.
Regards,
Mario
Hi mario_castanedahanks again for your reply.
If I used ZB3 as a stack version willl it be compatible with other stack versions ?
Is there any method to guarantee that I can make my system compatible with every possible zigbee device?
I want to try for example integrating Philips Hue to control it from my coordinator.
Are there any parameters I would need to know and take care of while coding my coordinator other than the profile type?
Thanks.
David
Hi David,
Yes, It should be compatible, but you have to be sure the Coordinator, in this case, has enabled the ZLL, then you have to share the key of the network that you want to add the external device.
Regards,
Mario
Hi mario_castanedahat's helpful thank you!
Finally is there any custom (device specific) settings I should take care of in my code other than the shared key ?
should I search for documents for each device I want to integrate and apply some settings ? maybe some custom messages to achieve some function ?
Many thanks
David
Hi David,
As you know, that is one of the features of Zigbee, interoperability.
There are also Zigbee stacks are not certified, don't count interoperability with these stacks. Nonetheless, You can be sure, if the device has a certified stack, you won't have any problem.
Regards,
Mario