Info on Energy detection scan in Zigbee

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Info on Energy detection scan in Zigbee

3,449 次查看
divyak
Contributor I

Hi,

I am using FRDM-KW40Z Zigbee.

During the energy detection scan, I get a 8bit value. how can I translate it to dB?

Is 25% a good threshold value for the energy during an energy detection scan?

标签 (2)
0 项奖励
回复
3 回复数

2,981 次查看
zigbee1
Contributor III

Here after is exactly what I getting from several router connected to the Zigbee controller. The information is collected via Mgmt_NWK_Update_notify message data.

Per channel, I'm so getting a value between 0 and 0xFE (while 0xFF stand for indicates there is too much interference on the channel as per the ZigBee PRO Stack documentation)

 Network Energy Level Report
 -----------------------------------------------
 nwkid     Tx  Failure   11   15   19   20   25   26
  ca62     40        0  171  172  162  161  179  175
  2d25     43        0  175  194  168  165  176  196
  f775     32        0  187  183  164  170  177  187
  9596     36        0  192  196  171  163  175  202
  eb73     30        0  180  184  161  170  180  187
  fc80     24        0  191  185  169  162  178  191
  83c2     23        0  204  210  205  206  190  207
  1f33     33        0  174  188  172  167  179  188
  0fc4     40        0  175  179  172  174  166  177
  aa38     28        0  187  189  180  177  179  191

Question:

- How to interprate those result. Should the reported energy-level measurements be as lower as possible to report a better channel or vice-versa ?

- Can we convert this reported energy-level measurements into db ?

I'm using JN5168

0 项奖励
回复

2,981 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Patrick,

Could you please provide more details about this?

What is the device that you are using? and how are you measuring this? 

Regards,

Mario

0 项奖励
回复

2,981 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Divya,

Did you mean 802.15.4? The KW40z doesn't support Zigbee.

dBm and RSSI are different units of measurement that both represent the same thing: signal strength. The difference is that RSSI is a relative index, while dBm is an absolute number representing power levels in mW (milliwatts).

Could you provide for information about your final application?

Hope it helps

Mario

0 项奖励
回复