Implementing serial protocol between host and control bridge.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Implementing serial protocol between host and control bridge.

1,441 次查看
kousikbarathwaj
Contributor I

In JN-AN-1194 (Zigbee Iot gateway application note) the document for control bridge, NXP have specified serial protocol and command sets to interact with the control bridge (zigbee module connected to the host) from the host through serial connection. In the accompanying documents for host they have used Jennet ip for translation between IPV6 and WPAN packets.

In our project there is no need for IPV6 translations.   From the linux host we have to interact with the control bridge(zigbee module connected to the host) through serial protocol.  Please suggest me on how this can be implemented.

Thanks in advance.

标签 (2)
0 项奖励
回复
0 回复数