Hello Mario,
Thanks for your reply.
As you know that I have also generated ticket regarding this issue and you replied on it. I also revert back on your feedback, but didn't get any feedback from you or NXP tech support. It might be possible that my reply mail is not reach to you due to external email. So, I am writing here.
Explanation of Problem:
I am integrating the Wireless UART and OTAP project code. I have used OTAP example code and add all required functions of Wireless UART to OTAP code. I am successfully able to send the serial data from NXP IOT application to KW36 module with this code. But not able to send serial data from KW36 module to NXP IOT application.
So, for this I have added the "lib_ble_5-0_host_cm0p.a" library file in to my code. And I got success to send and receive data from both side. It means, I am able to send serial data from KW36 module to NXP IOT application and vice versa.
But, after adding the "lib_ble_5-0_host_cm0p.a" library file, I am not able to update my firmware via OTAP. If I remove this library file from project, then able to update my firmware via OTAP. So, for this I need support from your/NXP side.
Questions:
1. Can you provide me the combine library file which supports both OTAP and Wireless UART functionality?
So, I can use it into my code.
OR
2. If possible, Can you provide me the source code for the all library files with its explanation document?
So, I can develop it as per my requirement.
Kindly help ASAP, because I am stuck in my project and I have to complete it in time.
Ticket Information:
- Project: Active Exhaust Module
- Case: 00260249
- Date Opened: 2/14/2020
- Subject: How to get the serial data from KW36 module to IOT application?
Thank you.