How to use Smart Energy Tunneling cluster without Application Level Security?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use Smart Energy Tunneling cluster without Application Level Security?

1,196 次查看
arthurpulatov
Contributor II

I use JN-AN-1135 project as template.
There is  presented Tunneling cluster between ESP and Plug Meter node.

I want to implement it on the second  Plug Meter node with another IEEE/MAC.

But when i do that i have expected problems with an Application Level Security.
In fact I do not need any security in my project, i need only   I need only a tunneling cluster (mechanizm which can transmit long payload throw the ZigBee network).

Can anyone help me?




标签 (1)
0 项奖励
回复
1 回复

1,050 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Arthur,

Could you please check the ZigBee PRO Stack User Guide JN-UG-3048?

5.7 Implementing ZigBee Security

5.7.2 Application-level Security Set-up

If security is enabled in a ZigBee network then network-level security is always used, while application-level security is optional. Security is enabled on a node via the device parameter Security Enabled in the ZPS Configuration Editor.

 http://www.nxp.com/documents/user_manual/JN-UG-3048.pdf 

Hope it helps.

Regards,

Mario

0 项奖励
回复