How to send a non-standard packet?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to send a non-standard packet?

跳至解决方案
1,880 次查看
sChameleoNz
Contributor III

I've been using SDK_2_6_4_JN5189DK6.

And I want to send and receive a non-standard 802.15.4 packet while using ZB.

How could I achieve this?

标签 (3)
0 项奖励
回复
1 解答
1,867 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

It is impossible to send the non-standard 802.15.4 packet. The zigbee frame header and tail is added by the lib that is invisible to us.

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,868 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

It is impossible to send the non-standard 802.15.4 packet. The zigbee frame header and tail is added by the lib that is invisible to us.

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------