How to send a non-standard packet?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to send a non-standard packet?

ソリューションへジャンプ
1,846件の閲覧回数
sChameleoNz
Contributor III

I've been using SDK_2_6_4_JN5189DK6.

And I want to send and receive a non-standard 802.15.4 packet while using ZB.

How could I achieve this?

ラベル(3)
0 件の賞賛
返信
1 解決策
1,833件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

It is impossible to send the non-standard 802.15.4 packet. The zigbee frame header and tail is added by the lib that is invisible to us.

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,834件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

It is impossible to send the non-standard 802.15.4 packet. The zigbee frame header and tail is added by the lib that is invisible to us.

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------