How to introduce WiFi capability in my system ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to introduce WiFi capability in my system ?

1,255件の閲覧回数
arvindpal
Contributor I

We have embedded devices with LPC2387 (ARM7) as MCU. Its firmware is based on FreeRTOS. Data rate requirement : minimal (Around 1-2 Mbps). We want to have Wifi capability in our device.Which of your devices will be best suited for our  requirements. We would like to have its code library and driver to be available ?

タグ(5)
0 件の賞賛
返信
1 返信

1,115件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Arvind,

unfortunately NXP doent snot develop  Wifi module, therefore we cannot provide a full solution.

However, you can find an exampe using Kinetis K22 and K64 MCUs with GT202 which is a Qualcomm solution. NXP provides such example in its Kinetis SDK v2.1 and above.

ESP8266 is another popular solution which you can incorporate to you FreeRTOS project. This module contains TCP/IP embedded stack.

 If you have any question please let me know.


Best regards,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信