How to enable AP mode on the QCA6174 radio on i.MX8?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable AP mode on the QCA6174 radio on i.MX8?

ソリューションへジャンプ
1,989件の閲覧回数
babarhashim
Contributor III

Can the QCA6174 radio on the i.MX 8 be used as an access point?

タグ(1)
0 件の賞賛
返信
1 解決策
1,807件の閲覧回数
babarhashim
Contributor III

The QCA6174 radio on the i.MX 8 does not operate in AP mode out of the box. 

If you want to enable the radio to operate in AP mode, the easiest way is to use SX-PCEAC2-EVK which includes the QCA6174 based module from Siles.

Silex has also tweaked the NXP BSP to enable soft AP mode so that customers can use this high performance radio as an access point. To learn more on the evaluation kit for the QCA6174 please visit the below link.

QCA6174 Evaluation 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,808件の閲覧回数
babarhashim
Contributor III

The QCA6174 radio on the i.MX 8 does not operate in AP mode out of the box. 

If you want to enable the radio to operate in AP mode, the easiest way is to use SX-PCEAC2-EVK which includes the QCA6174 based module from Siles.

Silex has also tweaked the NXP BSP to enable soft AP mode so that customers can use this high performance radio as an access point. To learn more on the evaluation kit for the QCA6174 please visit the below link.

QCA6174 Evaluation 

0 件の賞賛
返信