How many services and charactors can QN9020 support?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How many services and charactors can QN9020 support?

1,498件の閲覧回数
wysnewhope
Contributor I

I need transfer a data table which is not big, only 20 lines with 2 columns. I assigned a service for a line, with 2 charactors are for two columns. The first charactor is 4 bytes and the second charactor is 20 bytes. So there will be 20 services for the 20 lines data, with 2 charactors for each lines.

But when there are more than 5 services, the program will can't run normally. Even I modified the BLE_DB_SIZE, can't it up to 8 lines. How can I make it support to up to 20 lines?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,379件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Tonny,

the BLE_DB_SIZE is added in the equation to take care of the dynamic allocation of attribute database.

 Did you take as reference the QPPS example?

Regards,

Mario

0 件の賞賛
返信