How many services and charactors can QN9020 support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many services and charactors can QN9020 support?

1,503 Views
wysnewhope
Contributor I

I need transfer a data table which is not big, only 20 lines with 2 columns. I assigned a service for a line, with 2 charactors are for two columns. The first charactor is 4 bytes and the second charactor is 20 bytes. So there will be 20 services for the 20 lines data, with 2 charactors for each lines.

But when there are more than 5 services, the program will can't run normally. Even I modified the BLE_DB_SIZE, can't it up to 8 lines. How can I make it support to up to 20 lines?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,384 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Tonny,

the BLE_DB_SIZE is added in the equation to take care of the dynamic allocation of attribute database.

 Did you take as reference the QPPS example?

Regards,

Mario

0 Kudos
Reply