High Power RF FET for 155 - 165 MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

High Power RF FET for 155 - 165 MHz

1,082件の閲覧回数
mixtwitch
Contributor I

Hi, I'm wondering could you recommend the best NXP high power RF FET to use for marine VHF radio applications - 25W, 155 - 165 MHz. Would it be something similar to AFT05MS031N? And where would be the best place to get a quote, based in NZ?

Many Thanks,

Dave

0 件の賞賛
返信
1 返信

1,069件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Dave,

I hope all is great with you.

Based on your requirements, you are correct, the AFT05MS031N device is a great option for your design. You may also consider the AFT05MP075N device.

What do you mean with “get the quote”? I do recommend to request more information to your local distributor.

Note that you can download the S-Parameter or ADS/AWR model from the webpage in case they are useful for you.

diazmarin09_0-1657825874700.png

 

Regards,

David  

0 件の賞賛
返信