Flashing bootloader application on KW37/38/39

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flashing bootloader application on KW37/38/39

1,372 次查看
mahmoud_swaidan
Contributor III

Hello, 

We need your support in the following topic. 

The KW37/38/39 is used in our projects and need to be tested according to BT spec. in non-signaling mode. 

As I know, for Hardware verification (RF Performance), we need to flash the HCI_blackbox application to the target. 

According to NXP system engineer: Because the target is still blank, we should first flash the blootloader application (using th SWD signals) in order to use the UART and SPI interfaces 

1- Could you please provide a detailed explanation or AN which describes the steps how to flash the bootloader application to the target and then the hci_blackbox.

We have access to: 

PTA0 (SWD_DIO) / PTA1 ( SWD_CLK) 

PTC2 (UART_RX) / PTC3 (UART_TX).

2- Which connector need to be used to connect the IC (SWD) to the PC

Thanks and regards

M.Swaidan

标签 (3)
标记 (1)
0 项奖励
回复
1 回复

1,244 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Sorry for the inconvenience this might cause you, but as this product has not been released yet I do not have any information available to share with you, nonetheless, could you please reach your NXP contact for further information about this ?

 

Regards,
Estephania

0 项奖励
回复