Error 0x87 - ZPS_XS_E_NO_FREE_EXTENDED_ADDR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error 0x87 - ZPS_XS_E_NO_FREE_EXTENDED_ADDR

2,415件の閲覧回数
zigbee1
Contributor III

We are currently maintaining a  Zigbee controller out of JN5169.
We are using the JN-SW-4170 SDK.
We have of course a good understanding of JN-AN-1216
Application Note: JN-AN-1216 ZigBee 3.0 IoT Control Bridge,

 

Still facing 0x87 - ZPS_XS_E_NO_FREE_EXTENDED_ADDR. The documentation refer to "extended address table", but in none of the documentation this table is defined!

Here are the various parameter definition

MaxNumberNodes70
ActiveNeighbourTableSize50
RoutingTableSize70
AddressMapTableSize20
MacTableSize70
ChildTableSize5
DeviceTableSize70
ZNC_MAX_TCLK_DEVICES70

 

What is wrong ?

0 件の賞賛
返信
6 返答(返信)

910件の閲覧回数
BasWep
Contributor I

@mario_castaneda 

Hello, With have 21 routers in the zigbee network I have also code: ERROR: Extended status 87 (ZPS_XS_E_NO_FREE_EXTENDED_ADDR)

This is my settings: app_zps_cfg.h
#define ZPS_ADDRESS_MAP_TABLE_SIZE 100
#define ZPS_MAC_ADDRESS_TABLE_SIZE 100

0 件の賞賛
返信

892件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @BasWep,

Is it possible that you could create a new community post with this issue? one of my colleagues will check this problem.

Regards,

Mario

0 件の賞賛
返信

2,400件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @zigbee1,

What is happening when you get this error?

The coordinator is not accepting a new device? when you are trying to remove a device?

Regards,

Mario

0 件の賞賛
返信

2,394件の閲覧回数
zigbee1
Contributor III

nothing is done!, no addition nor removal of devices. I just have somehow a stable network at least it behaves like that and get those asynchronous messages.

Could you please clarify what this table is ""extended address table"" as there is no definition of such table in none of the NXP manual

0 件の賞賛
返信

2,370件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @zigbee1,

The value that the free extended address depends on the sum of the mac table and the map table.

Please try to increase let me know if you are still facing this error.

Regards,

Mario

0 件の賞賛
返信

1,343件の閲覧回数
BasWep
Contributor I
Hello, With have 21 routers in the zigbee network I have also code: ERROR: Extended status 87 (ZPS_XS_E_NO_FREE_EXTENDED_ADDR)

This is my settings: app_zps_cfg.h
#define ZPS_ADDRESS_MAP_TABLE_SIZE 100
#define ZPS_MAC_ADDRESS_TABLE_SIZE 100
0 件の賞賛
返信