End device and Router device capacity is 2, which is not as per the Specification.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

End device and Router device capacity is 2, which is not as per the Specification.

2,328件の閲覧回数
vihang_jani
Contributor I

Hi,

      Sometimes I get End Device and router capacity is 2 in ZPS_EVENT_NWK_DISCOVERY_COMPLETE Pkt  sometimes it can give proper value, have anyone know the reason of this issue?

As per Zigbee specification ( Document 053474r20)

Router Capacity

TYPE : Boolean
Valid Range : TRUE(1) or FALSE(0)

Description : This value is set to true if the device is capable of accepting join requests from router-capable devices and set to FALSE otherwise.

EndDeviceCapacity

TYPE : Boolean 
Valid Range : TRUE(1) or FALSE(0)

Description : This value is set to true if the device is capable of accepting join requests from end devices and set to FALSE otherwise.



NOTE  : I have attached log for your reference and am using JN-SW-4166 SDK.

Set Channel to 11

vSL_WriteMessage(32793, 1, 93)

Scan is over Channel
vEZ_ClearDiscNT done
vAttemptDiscovery :- Discovery API Status =0
EZ_STATE = 0
APP_ZpsEventTask sStackEvent.eType : 0x000a
ZPS_EVENT_NWK_DISCOVERY_COMPLETE

vSL_WriteMessage(32791, 63, 54)

******eNodeState : 0x02*****sStackEvent.eType : 0xa
eGetEZModeState = 3 , u8JoinAttempts = 1
ZPS_EVENT_NWK_DISCOVERY_COMPLETE......NWK Found, Count = 4
vEZ_SortAndSaveNetworks
***Saving Open NWK ExPANID = 0xdf964fec0a52d931
*vEZ_SortAndSaveNetworks sEZModeData.u8DiscoveredNwkCount = 1
u8DiscoveredNwkCount : 1
u8JoinIndex : 0
u64ExtPanId : 0xX
u8EndDeviceCapacity : 2
u8LogicalChan : 11
u8PermitJoining : 1
u8RouterCapacity : 2
u8StackProfile : 2
u8ZigBeeVersion : 2
Join Network API Success 0

vSL_WriteMessage(32800, 16, 1a)

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

1,797件の閲覧回数
vihang_jani
Contributor I

Hi Mario,

I am using JN-SW-4364-ZigBee-SmartEnergy1.x1721 and JN-AN-1207-Smart-Energy-HAN-Solutions-Network-CoProcessor 

0 件の賞賛
返信

1,797件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Vihang,

Could you please check the Zigbee SDK  that we provide?

Support Resources for JN516x MCUs|NXP 

pastedImage_2.png

Regards,

Mario

0 件の賞賛
返信

1,797件の閲覧回数
vihang_jani
Contributor I

Good Morning Mario,

I am using Application Note JN-SW-4364-ZigBee-SmartEnergy1.x-v1721 and JN-AN-1207-Smart-Energy-HAN-Solutions-Network-CoProcessor.

0 件の賞賛
返信

1,797件の閲覧回数
vihang_jani
Contributor I

Application Note is JN-SW-4364-ZigBee-SmartEnergy1.x-v1721

0 件の賞賛
返信

1,797件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Vihang,

I'm sorry. I could not find the Application note that you are referring to.

Could you please point me the link of the application note that you are mentioning?

Regards,

Mario

0 件の賞賛
返信

1,797件の閲覧回数
vihang_jani
Contributor I

Hi Mario,

I am using JN-SW-4364-ZigBee-SmartEnergy1.x1721 and JN-AN-1207-Smart-Energy-HAN-Solutions-Network-CoProcessor

0 件の賞賛
返信