Create a log file of the packet transactions using KW01's Radio Utility Application_Video

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Create a log file of the packet transactions using KW01's Radio Utility Application_Video

1,563件の閲覧回数
CesarM
Contributor III

When performing tests on a communication link there are scenarios where it is very useful to have a data log of the packet transactions, where you can have access to read several variables that correspond to the communication like: preamble settings, sync word details,  RSSI, number of packet received, among others.


This video will guide you to enable and save a log file of the packet transactions using the GUI-based Radio Utility Application demonstration.


このビデオは削除されました
(マイビデオを表示)

ラベル(1)
0 件の賞賛
返信
0 返答(返信)