Confirmation timeout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Confirmation timeout

跳至解决方案
1,666 次查看
jictannu
Contributor III

I find this in KW36 SDK ble_general.h:

typedef enum
{

   ...

   gGattClientConfirmationTimeout_c = gGattStatusBase_c | 0x08, /*!< No Confirmation was received from the Client after a Server Indication. */

   ...

} bleResult_t;

However, I could not find where returns gGattClientConfirmationTimeout_c . GattServer_SendInstantValueIndication always returns gBleSuccess_c even if I does not get gEvtHandleValueConfirmation_c. So how could I know that I didn't receive Confirmation?

标签 (3)
0 项奖励
回复
1 解答
1,520 次查看
xing_chang
NXP Employee
NXP Employee

Hi Xinyu,

Please note that related events are handled in BleApp_Gatt ServerCallback ().

Please refer to "Bluetooth® Low Energy Application Developer’s Guide".

There is an important difference between sending Notifications and Indications: the latter can only be sent one at a time and the application must wait for the Client Confirmation (signaled by the gEvtHandleValueConfirmation_c Server event, or by a gEvtError_c event with gGattClientConfirmationTimeout_c error code) before sending a new Indication. Otherwise, a gEvtError_c event with gGattIndicationAlreadyInProgress_c error code is triggered. The Notifications can be sent consecutively.

在原帖中查看解决方案

1 回复
1,521 次查看
xing_chang
NXP Employee
NXP Employee

Hi Xinyu,

Please note that related events are handled in BleApp_Gatt ServerCallback ().

Please refer to "Bluetooth® Low Energy Application Developer’s Guide".

There is an important difference between sending Notifications and Indications: the latter can only be sent one at a time and the application must wait for the Client Confirmation (signaled by the gEvtHandleValueConfirmation_c Server event, or by a gEvtError_c event with gGattClientConfirmationTimeout_c error code) before sending a new Indication. Otherwise, a gEvtError_c event with gGattIndicationAlreadyInProgress_c error code is triggered. The Notifications can be sent consecutively.