Building project on JN5168

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Building project on JN5168

ソリューションへジャンプ
1,838件の閲覧回数
gibish
Contributor II

Hello

I have some project, based on 1190-JenNet-IP-Application-Template, and use JN5168.

Now project includes one coordinator and three routers.

When I change the code for my coordinator, I build the binary file and program coordinator.

But routers refuse to connect to new network and I have to build new binary file for router and reprogram all routers.

Parameters CONFIG_NETWORK_ID, CONFIG_PAN_ID and CONFIG_SCAN_CHANNELS have constant values.

Please, give me an advice. Which additional parameters have I to do constant to avoid reprogramming all routers in case, when I build the binary file and program only coordinator?

タグ(1)
0 件の賞賛
返信
1 解決策
1,584件の閲覧回数
janibal
Contributor II

When you load the program into coordinator device, you have to preserv EEPROM in the setup of programmer. if you don't, you will delete the info about the network, hence the coordinator will not remember its children. Good luck

元の投稿で解決策を見る

1 返信
1,585件の閲覧回数
janibal
Contributor II

When you load the program into coordinator device, you have to preserv EEPROM in the setup of programmer. if you don't, you will delete the info about the network, hence the coordinator will not remember its children. Good luck