Bluetooth OPP fails in Android Lollipop 5.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bluetooth OPP fails in Android Lollipop 5.0.0

917件の閲覧回数
anjalikkrishna
Contributor III

Hi,

I am using  Android 5.0 BSP to test Bluetooth . WG7831-D0  Wi-Fi BT Combo module from Jorjin is being used  . When I test the OPP from remote phone to the host , the file transfer is success . But when I try to send the file from the host to the phone, the transfer fails. The phone is not even getting the  " Accept the file" prompt. Later the host hangs and the kernel crashes and reboots.

Has anyone experienced the same issue?

Thanks & Regards,

Anjali

ラベル(1)
0 件の賞賛
返信
0 返答(返信)