Beyondstudio with sharedrive (network)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Beyondstudio with sharedrive (network)

2,329 次查看
zigbee1
Contributor III

I'm having a problem to get a setup with some of the SDK and the workspace on a remote drive.

Here is a screenshoot of the Build errors. It looks like the z: drive is not recognized

I have also use mklink /d to create symbolic links but this doesn't help !

Any suggestions, recommendation on how/what to do ?

1 回复

2,300 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Patrick, I hope you're doing well!

 

We recommend using the default path of installation for the BeyondStudio IDE, as changing it can cause issues like the ones you're experiencing.

 

Could you please take a look at the following document for information about BeyondStudio Common Errors?

 

Please let me know if you need any more information.

 

Best regards,

Sebastian