ATT_MTU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ATT_MTU

2,007 Views
koonlee
Contributor I

In NXP’s KW40Z_Connectivity_Software_1.0.1 package, there is a wireless_uart_demo project under BLE example directory. Our goal is to modify this project such that it can transmit 1000 BLE packets with 250 bytes data.

 

I use the wireless_uart_demo project and create two copies; one for receiver and one for sender. The sender project will transmit 1000 packets and the receiver will display the packets it receives in the Shell. Next, in sender project, I modify UartStreamFlushTimerCallback function in app.c (see attachment: app_Sender.c) and in receiver project, I modify BleApp_GattServerCallback function in app.c (see attachment: app_RX.c). For both sender and receiver projects, I add GattClient_ExchangeMtu command in BleApp_StateMachineHandler function so that it can expand ATT_MTU to 250.

 

When I select temp[20] and bytesRead=20 in UartStreamFlushTimerCallback function in sender project, receiver project is able to display all 1000 packets in the Shell. However, if I select temp[30] and bytesRead=30, receiver project doesn’t display any packet. However, when I use a sniffer, the sniffer is able to capture the 30 bytes data packet (see attachment: sniffer_capture.png) and the ATT_Exchange_MTU request and response.

 

Did I miss any step to enable large payload?

Tags (3)
0 Kudos
Reply
1 Reply

1,734 Views
koonlee
Contributor I

Issue solved.

0 Kudos
Reply