how to run the KW2xD-SMC.exe on the TWR-KW24D512?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to run the KW2xD-SMC.exe on the TWR-KW24D512?

Jump to solution
1,237 Views
kentachang
Contributor I

Hello,

I have a TWR-KW24D512 and a USB-KW24D512 , but I am a new user, could you please let me know Is there a demo-example to run (communication TxRx) this two Kits?

Best Regards,

Kenta

0 Kudos
1 Solution
1,057 Views
antonioconcio
NXP Employee
NXP Employee

Hi Kenta,

As mentioned in the other post regarding 802.15.4 MAC stack, the Freescale connectivity stacks are built on top of the KSDK (Software Development Kit for Kinetis MCUs).

In this case the first step is to install the Kinetis SDK version 1.2.0 using the installation package from the Freescale website.

After completing the KSDK installation procedure, you can install the SMAC stack (KW2xD-SMAC.exe).

I am attaching the Quick Start Guide for the Freescale MKW2xD SMAC Software inluded in the package at the location C:\Freescale\KW2xD_SMAC\doc (default path). The document walks you through all the steps needed to install SDK and SMAC stack as well as explaining how to build and run the application on both TWR-KW24D512 and USB-KW24D512 boards.

Let me know if you face any issue,

Antonio

View solution in original post

0 Kudos
1 Reply
1,058 Views
antonioconcio
NXP Employee
NXP Employee

Hi Kenta,

As mentioned in the other post regarding 802.15.4 MAC stack, the Freescale connectivity stacks are built on top of the KSDK (Software Development Kit for Kinetis MCUs).

In this case the first step is to install the Kinetis SDK version 1.2.0 using the installation package from the Freescale website.

After completing the KSDK installation procedure, you can install the SMAC stack (KW2xD-SMAC.exe).

I am attaching the Quick Start Guide for the Freescale MKW2xD SMAC Software inluded in the package at the location C:\Freescale\KW2xD_SMAC\doc (default path). The document walks you through all the steps needed to install SDK and SMAC stack as well as explaining how to build and run the application on both TWR-KW24D512 and USB-KW24D512 boards.

Let me know if you face any issue,

Antonio

0 Kudos