how to extract MAC address ? (JN5169 )

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to extract MAC address ? (JN5169 )

2,107 Views
lightwei
Contributor I

Hi:

  how to  extract MAC address ? (JN5169 )

for example

微信截图_20181108161554.png

Tags (1)
3 Replies

1,698 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Gan Wei

A unique MAC Address is programmed by NXP into the internal Flash and is what is used by default by the stack.

ZPS_u64AplZdoGetIeeeAddr ()

This function obtains the 64-bit IEEE (MAC) address of the local node.

Returns: 64-bit IEEE/MAC address obtained

For a better reference: ZigBee 3.0 Stack User Guide

We also provide a Production Flash programmer tool which can be used to program MAC address one time into the specific flash location.

Support Resources for JN516x MCUs

JN-SW-4107 Utility for loading built applications into JN51xx devices in a production environment. For details, refer to the User Guide JN-UG-3099.

Regards,

Mario

485 Views
AlbertoGallegos
Contributor I

 

Sorry If this is an old post and If should make a new one.
Regarding this question, How do I access the device's extended address value without the zigbee stack?


In essence, I want to be able to read aExtendeAddress and other MAC constant values from my program.
(For example JN-AN-1174)

0 Kudos
Reply

1,698 Views
lightwei
Contributor I

HI Mario:

This problem has been resolved

thank you very much

Regards

gan wei

深圳市中龙通电子科技有限公司

企业远景:中国射频模块第一品牌!

企业使命:创造精彩的信息生活!

─────────────────────

地址:深圳市宝安区沙井街道南浦路253号蚝三林坡坑第一工业区B4栋

电话: 86-755-81449957 (845) 传真: 86-755-81449967

手机:18320876889

邮箱:gps.pie@cdtech.cn

网址:http://www.cdtech.cn

发件人: mario_castaneda

发送时间: 2018-11-15 02:32

收件人: gan wei

主题: Re: - Re: how to extract MAC address ? (JN5169 )

NXP Community

Re: how to extract MAC address ? (JN5169 )

reply from Mario Ignacio Castaneda Lopez in Wireless Connectivity - View the full discussion

Hi Gan Wei

A unique MAC Address is programmed by NXP into the internal Flash and is what is used by default by the stack.

ZPS_u64AplZdoGetIeeeAddr ()

This function obtains the 64-bit IEEE (MAC) address of the local node.

Returns: 64-bit IEEE/MAC address obtained

For a better reference: ZigBee 3.0 Stack User Guide

We also provide a Production Flash programmer tool which can be used to program MAC address one time into the specific flash location.

Support Resources for JN516x MCUs

JN-SW-4107 Utility for loading built applications into JN51xx devices in a production environment. For details, refer to the User Guide JN-UG-3099.

Regards,

Mario

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in Wireless Connectivity by email or at NXP Community

Following Re: how to extract MAC address ? (JN5169 ) in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos
Reply