how to configure 8KB flexram as general RAM at KW36

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to configure 8KB flexram as general RAM at KW36

687 Views
zhi_wang
Contributor III

hi someone,

will the FlexRAM could be configured as general RAM at KW36 platform?

there is no demo code nor help doc about this issue. 

 

Regards,

 

Labels (2)
0 Kudos
1 Reply

593 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. Yes, the FlexRAM can be used as a traditional RAM.

From the Reference Manual (Chapter 29):

Ricardo_Zamora_1-1638921976013.png

 

Could you please check section 29.4.11.17?

The Set FlexRAM Function command changes the function of the FlexRAM.

 

Hope this helps.

Best Regards,

Ricardo

0 Kudos