beyond studio (jn5169)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

beyond studio (jn5169)

756 Views
brengel
Contributor I

hello,

i have a problem to compile my application on windows 10

(JN-AN-1216-Zigbee-3-0-IoT-ControlBridge-v1011)

beyond studio Build 1308

Generating binary ...
/c/NXP/bstudio_nxp/sdk/Tools/ba-elf-ba2-r36379/bin/ba-elf-objcopy -j .version -j .bir -j .flashheader -j .vsr_table -j .vsr_handlers -j .ro_mac_address -j .ro_ota_header -j .ro_se_customData -j .rodata -j .text -j .data -j .bss -j .heap -j .stack -S -O binary ZigbeeNodeControlBridge_JN5169_GP_Proxy_FULL_FUNC_DEVICE_1000000.elf ZigbeeNodeControlBridge_JN5169_GP_Proxy_FULL_FUNC_DEVICE_1000000.bin
/c/NXP/bstudio_nxp/sdk/JN-SW-4170/Tools/Memsize/memsize.exe /c/NXP/bstudio_nxp/workspace/JN-AN-1216-Zigbee-3-0-IoT-ControlBridge-v1011/JN-AN-1216-Zigbee-3-0-IoT-ControlBridge/Build/ZigbeeNodeControlBridge/ZigbeeNodeControlBridge_JN5169_GP_Proxy_FULL_FUNC_DEVICE_1000000.elf /c/NXP/bstudio_nxp/workspace/JN-AN-1216-Zigbee-3-0-IoT-ControlBridge-v1011/JN-AN-1216-Zigbee-3-0-IoT-ControlBridge/Build/ZigbeeNodeControlBridge/ZigbeeNodeControlBridge_JN5169_GP_Proxy_FULL_FUNC_DEVICE_1000000_NOLTO.map ZigbeeNodeControlBridge.json
Error loading Python DLL 'C:/Users/ybren/AppData/Local/Temp\_MEI84722\python36.dll'.
LoadLibrary: Paramètre incorrect.

if you have a idea ?

else can i migrate my project on MCUxexpresso IDE ?

Sinceraly

yann

0 Kudos
Reply
1 Reply

697 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Yann,

Generating binary ...
/c/NXP/bstudio_nxp/sdk/Tools/ba-elf-ba2-r36379/bin/ba-elf-objcopy -j .version -j .bir -j .flashheader -j .vsr_table -j .vsr_handlers -j .ro_mac_address -j .ro_ota_header -j .ro_se_customData -j .rodata -j .text -j .data -j .bss -j .heap -j .stack -S -O binary ZigbeeNodeControlBridge_JN5169_GP_Proxy_FULL_FUNC_DEVICE_1000000.elf ZigbeeNodeControlBridge_JN5169_GP_Proxy_FULL_FUNC_DEVICE_1000000.bin

Your compile process was success.

Please ignore the python issue.

Regards,

Mario

0 Kudos
Reply