Hello,
I have this function, in the End Device SDK Example of MCUXpresso, to send a dummy write attribute command to a custom attributes arleady created in another node in the network with that Short Address:
BDB_teStatus APP_sendData(bool bWriteAttResponse){
BDB_teStatus eStatus;
if ((sNodeState.eNodeState == E_RUNNING) && (bFailToJoinNode == FALSE))
{
tsZCL_Address sAddress;
sAddress.eAddressMode = E_ZCL_AM_SHORT;
sAddress.uAddress.u16DestinationAddress = 0xAED9;
uint16 u16ClusterId = 0x0b04;
uint16 u16ManId = 0x1037;
uint8 u8SourceEndpoint = 1;
uint8 u8DestEndpoint = 1;
uint8 bServerToClient = FALSE;
uint8 u8SeqNum;
uint8 bManSpecific = TRUE;
uint8 u8NumbAttributes = 2;
uint8 u8ZCLPayload1[] = {0x12, 0x34};
uint8 u8ZCLPayload2[] = {0x56, 0x78};
tsZCL_WriteAttributeRecord pu16AttributeRequestList[2];
pu16AttributeRequestList[0].eAttributeDataType = E_ZCL_INT16;
pu16AttributeRequestList[0].u16AttributeEnum = 0x0b00;
pu16AttributeRequestList[0].pu8AttributeData = u8ZCLPayload1;
pu16AttributeRequestList[1].eAttributeDataType = E_ZCL_INT16;
pu16AttributeRequestList[1].u16AttributeEnum = 0x0a00;
pu16AttributeRequestList[1].pu8AttributeData = u8ZCLPayload2;
if(bWriteAttResponse){
eStatus = eZCL_SendWriteAttributesRequest (u8SourceEndpoint,
u8DestEndpoint,
u16ClusterId,
bServerToClient,
&sAddress,
&u8SeqNum,
u8NumbAttributes,
bManSpecific,
u16ManId,
pu16AttributeRequestList);
}else{
eStatus = eZCL_SendWriteAttributesNoResponseRequest (u8SourceEndpoint,
u8DestEndpoint,
u16ClusterId,
bServerToClient,
&sAddress,
&u8SeqNum,
u8NumbAttributes,
bManSpecific,
u16ManId,
pu16AttributeRequestList);
}
}else{
}
return eStatus;
}
It works fine when I call the function from the button pressed case in the end device task:
as sniffer tool shows:
But if i send the same command from my custom task:
Creating the taks:
Sending from the Custom Task:
It doesn't work anymore and event triggers the watchdog.
What am I missing or which is the correct way to do this??
Thanks
Hi Alejandro,
Why do you have a for loop? It is a big delay, did you try to enable that specific cluster?
I am assuming that your custom, you could create an event in the code that sends the data that you want.
Regards,
Mario
Hi Mario,
Thanks for your replay,
The loop is just for testing right now.
What I'm try to do is get the data from a sensor, that I allready have working, send the data to specific cluster, that It's allready created too, put to sleep the end device for some specific time, say one minute or five minutes, then wake up and repeat the clycle, so that's the way i'm starting and really want to know the best way to achieve it. The cluster part is allready working when the event is from a pressed button, but I need a timer event.
Regards
Hi Alejandro,
Instead of the time event, you could bind your devices, at the beginning the end device will set up the binding endpoints that you want. In other words, the end device will report to his parents for any change or every specific time.
https://www.nxp.com/docs/en/user-guide/JN-UG-3113.pdf
2.6.2 Binding
Regards,
Mario