Zigbee 3.0 : The coordinator's address map information is not updated.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Zigbee 3.0 : The coordinator's address map information is not updated.

611 次查看
seunghokims
Contributor III

Coordinator - JN-AN-1216-Zigbee-3-0-IoT-ControlBridge

Router - 1

Ed - 1  (Router's child)

 

1. We joined with 1 coordinator, 1 router (0x3a09), and 1 Ed (0x005e) (Router's child).

 

2. vDisplayNWKTransmitTable();
- The router is not visible in the address map.

Routing Table Size 255
Status: 0, Short Address: 3a09, Next Hop: 3a09
Status: 4, Short Address: 5e, Next Hop: 3a09

Address Map Size: 10
Short Addr: 005e, Ext Addr: 00158d0002d53eae,
Short Addr: fffe, Ext Addr: 0000000000000000,
Short Addr: fffe, Ext Addr: 0000000000000000,

 

3. Ed (0x005e) sends a leave command
- Log
Src          Dest
0x005e    Broadcast             Leave
0x3a09    0x0000                  Update Device

 

4. vDisplayNWKTransmitTable();
- When a router's child is left, it is not removed from the coordinator's address map
Address Map Size: 10
Short Addr: 005e, Ext Addr: 00158d0002d53eae,
Short Addr: fffe, Ext Addr: 0000000000000000,
Short Addr: fffe, Ext Addr: 0000000000000000,
Short Addr: fffe, Ext Addr: 0000000000000000,

0 项奖励
1 回复

589 次查看
seunghokims
Contributor III

How can I delete it from the address map

0 项奖励