ZigBee Test Client on OM15020/JN5169

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ZigBee Test Client on OM15020/JN5169

873 Views
cmrlourenco
Contributor I

Can the OM15020 USB dongle be used as a ZigBee Test Client?

I've downloaded BeeKit, but it doesn't seem to be compatible with the dongle's MCU (JN5169).

Is there a ZTC-enabled firmware available for the dongle in question?

I'm specifically interested in communicating with the device using serial over USB in order to send and receive ZigBee commands.

Thanks in advance.

Labels (1)
0 Kudos
1 Reply

579 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

As you know the Beekti is for the KW24 products.

But you can take a look to the Control Brigde with the ZGUI. Please take a look to the JN-AN-1216, and look up to the JN-AN-1216-ZigBee-3-0-IoT-ControlBridge-UserGuide.

C:\NXP\bstudio_nxp\workspace\JN-AN-1216-Zigbee-3-0-IoT-ControlBridge\Doc

And the GUI

C:\NXP\bstudio_nxp\workspace\JN-AN-1216-Zigbee-3-0-IoT-ControlBridge\Tools\TestGUI

Hope it helps.

Best Regards,

Mario

0 Kudos