Writing multiple tags (NTAG) with PC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Writing multiple tags (NTAG) with PC

414 Views
MikhailUz
Contributor I

Knowing that there is a solution for a mobile phone device to write multiple tags in a row, I would like to ask if there is a ready solution for PC (using a reader/writer) to write multiple tags and record/log their data (UID and status) for future use.

Is there a ready solution using the TagXplorer or any ready script for the action?

The purpose is to have a conveyor attached to the reader/writer to be able to set the same info and settings to all the NTAG213 tags by passing them by the writer.

0 Kudos
1 Reply

403 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

We have several readers that can achieve the purpose, it will depend on the tag protocol you are using the reader to use,. You can check our available readers in this page.

In this case, we do not have a ready solution as requested, there is the need for every customer to implement their application , still, you can check as well in the RFID Ecosystem for a solution provider for your needs.

Regards,

Estephania

0 Kudos