WiFi Channel State Information (CSI) Extraction For IW612

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WiFi Channel State Information (CSI) Extraction For IW612

968 Views
abhayrjoshi
Contributor I

Dear Team,

Does the IW612 support WiFi CSI extraction in the 2.4 and 5 GHz band? If yes, is there any logging already setup (or SDK code) available for FreeRTOS? If not, can you please any alternative modules that support CSI extraction?

Thanks,
Abhay

0 Kudos
Reply
3 Replies

941 Views
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @abhayrjoshi 

 

Currently, our newest SDK 2.15 only support 88w8987 to enale CSI. To enable CSI, add CONFIG_CSI to /source/wifi_config.h in demo application wifi_wpa_supplicant.

shaun_wu_1-1706514529323.png

 

shaun_wu_0-1706514498115.png

 

0 Kudos
Reply

919 Views
abhayrjoshi
Contributor I
Thank you for the kind update. I see for the 88w8987, the interface is SDIO 3.0. Would you have any recommended host that supports an RTOS driver for the chipset for CSI extraction?
0 Kudos
Reply

912 Views
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @abhayrjoshi 

 

All platforms support your requests, you could select one:

i.MX RT Series: MCU/Applications Crossover MCUs | Arm® Cortex®-M7 | NXP Semiconductors

 

Best Regards

Shaun

0 Kudos
Reply