I am running a build of Linux 4.1.15-2.0.1 on a system with an NXP i.MX 6ULL processor. The system has a Murata LBEE5KL1DX WiFi / Bluetooth module. That module seems to work perfectly for my usual applications, but I need to do some low level tests of the module's radio. To carry out those tests, I am attempting to run the wl utility in WLTEST mode.
I have the following files:
root@XXXXXXXX:/lib/firmware/bcm# ls
BCM43430A1.1DX.hcd bcmdhd.cal fw_bcmdhd.bin fw_bcmdhd_apsta.bin fw_bcmdhd_mfgtest.bin
root@XXXXXXXX:/lib/firmware/bcm#
The wl utility seems to work fine when it uses (by default) the fw_bcmdhd.bin file:
root@XXXXXXXX:~# wl ver
1.107 RC5.0
wl0: Dec 29 2015 15:56:15 version 7.45.41.24 (r608913) FWID 01-4e412465
root@XXXXXXXX:~#
To run the wl utility in WLTEST mode, I was told to copy fw_bcmdhd_mfgtest.bin to fw_bcmdhd.bin. I copied the file, rebooted the machine, and entered wl ver, but it appears to hang the system. No output results from the command and the command prompt does not reappear. Do I need a different version of any of the files that I listed above?
Hi Jason,
See below, please!
https://wireless.murata.com/products/rf-modules-1/wi-fi-bluetooth/type-1dx.html
So you can ask for help on Space: Wi-Fi/Bluetooth for Linux and Android | Cypress Developer Community .
Have a nice day!
BR,
Weidong