Why can't port NFC sdk to efr32 (mifare plus example)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why can't port NFC sdk to efr32 (mifare plus example)?

568 Views
ivan_kryvosheia
Contributor I

I use nfc sdk on pn5180 
and successfuly ported mifare classic example to efr32.
So I can read, write cards etc.

The second goal is mifare plus. But nothings works.
Can it be because of compiling?
I mean, the project in MCUexpresso uses its own
arm-none-eabi and some library along with 

-D__CODE_RED
-D__REDLIB__
-specs=redlib.specs

What is it and can it be the reason?
0 Kudos
1 Reply

553 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @ivan_kryvosheia 

It seems the same question with the other case and I answered the question via the case. If any question please kindly let me know.

Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos