White List

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

White List

1,282 次查看
alejandropérez
Contributor II

1. Where is the white list?

2. Would be possibe to add a device without bonding or pairing previously?

Thanks in advance

标签 (2)
2 回复数

1,027 次查看
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Alejandro Pérez,

You can use the Gap_AddDeviceToWhiteList() function to add devices to the white list, and then configure the filter policy of the scanning parameters in the gScanParams structure to scan using the white list (gScanWithWhiteList_c).

The demo examples add the bonded devices to the whitelist, but you can manually add devices without being previously bonded.

Let me know if you have any question.

Regards,

Gerardo

1,027 次查看
alejandropérez
Contributor II

Hello Gerardo Rodriguez,

Now it seems that there is a limit on the maximum number of elements I can include in the whitelist... I can only use 7 nodes... node number 8 is rejected.

Please, could you help me on this topic?

Thanks in advance

Regards,

Alejandro

0 项奖励