Where the file ZigbeeControlBridge_JN5169.bin can be downloaded?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where the file ZigbeeControlBridge_JN5169.bin can be downloaded?

438 Views
pierre_dupont
Contributor I

I'm following the applicaiton note : JN-AN-1223. 

On Page 2, we need to download the firmware : ZigbeeControlBridge_JN5168.bin

Where should I download this file?

Labels (1)
Tags (1)
0 Kudos
1 Reply

399 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Philippe, I hope you're doing well!

 

Precompiled binary files for the control bridge firmware are included in the JN-AN-1223 Application Note, in the following path:

 <C:\NXP\bstudio_nxp\workspace\JN-AN-1223-ZigBee-IoT-Gateway-Control-Bridge-v1014\Build\bin>

 

If, for some reason, the folder is empty, like after a project clean up, the files can be re-compiled and generated by building the project using the BeyondStudio IDE.

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

0 Kudos