Hi
I am working on ZHA 1.2 & JN-AN-1223_ZigBee IoT Gateway Control Bridge_V1014.
Gateway Control Bridge is being used as a coordinator.
The coordinator and two routers are connected as shown.
(0xa529 is a child of 0x489e)
When Router(0xa529) tries to take Leave, the coordinator wants to receive the Command. (Update Device : Device Left)
When 0xa529 is leave from 0x489e,
Coordinator wants to receive any information.
Is there any way?
Hi Mario
Yes, I know.
As in the picture below (Router #1 = coordinator's child , Router#2 = router's child )
When the Router #2 is leave, Router #1 receive a message. (ZPS_EVENT_NWK_LEAVE_INDICATION)
However, this message does not appear in the coordinator at this time.
In the picture, the coordinator receive Command. (Update Device : Device Left)
As you said ZPS_EVENT_NWK_LEAVE_INDICATION,
I want to receive this Command. (Update Device : Device Left).
Thank you for your answers.
Hi Mario
Yes, this action was confirmed.
This action was received directly from router's child.(short Address:0xD0E1)
What I'm talking about is an environment where the coordinator can not receive a message directly from router's child.
Installed at a distance where the coordinator can not communicate directly with the end Device.
So I want to receive APS Command. (Update Device : Device Left)
- My current test environment
The coordinator is located in the shield box.
Hi Mario
We manufacture smart home systems.
Use a coordinator to manage the router and the ED device.
In large houses, devices are sometimes located away from the coordinator.
In such cases, the devices can not communicate directly with the coordinator and must pass through the router.
The situation is as follows.
1. Device_A is located at a distance from which it can not communicate directly with the coordinator.
2. Join the device_A to the router.
3. The information of the child(device_A) joined in the router is confirmed
by the ZPS_ZDP_DEVICE_ANNCE_REQ message.
4. Leave directly from device_A by user.
5. device_A broadcast Leave nwk_message.
6. The Router receives Leave nwk_message.
7. The coordinator does not receive the Leave nwk_message. (Because it is too far)
8. You can see the APS Command(Update Device : Device Left) in the sniffer.
9. I want the coordinator to receive APS Command(Update Device : Device Left).
- Because, our system must know if a devices exists.
The image below is what you answered.
ZPS_EVENT_NWK_LEAVE_INDICATION message occurs when Leave nwk_data is received.
Thank you.
Hi Seung Ho Kim,
As you know, the update device is an APS command ID
When the coordinator handles the APS data indication, you can get the payload with the PDUM_pvAPduInstanceGetPayload. JN51xx Core Utilities User Guide v1.1
As the coordinator is sending the acknowledge you can work with that specific command and with the device status.
Mario
Hi Mario Ignacio Castaneda Lopez
When I get the data in Update Device as you say, I find that the gateway doesn't receive APS data indication, so I can't extract the data you're talking about. My situation is the same as the description above. I use JN-AN-1216 as coordinator and SDK as JN-AN-4170.
Have you ever been tested? Are you sure the coordinator can get that?
Hi,Mario Ignacio Castaneda Lopez
Thank you for your reply.
My End device is connected to the network via a router.
I use this function ZPS_eAplZdoLeaveNetwork in the End device to apply to leave the network, At this point, the router can receive zps_EVENT_NWK_LEAVE_INDICATION. But the coordinator didn't get any instructions.
I read your reply, Your mean is when the coordinator handles the APS data indication, you can get the payload with the PDUM_pvAPduInstanceGetPayload.
But when the coordinator receives the update device, The coordinator didn't get any instructions example
Hi 天恒 韩,
Could you please submit a new community post with this question?
Also, Could you please attach the sniffer log of this? I will get back there.
What is the AN that you are working on?
Regards,
Mario
Hi Mario
Router is DimmableLight of JN-AN-1189.
ED is also DimmableLight.
What I want to know is that when a router's child is leave,
router receives ZPS_EVENT_NWK_LEAVE_INDICATION from router's child .
The router sends the Update device command to the coordinator when its child left.
I would like to process the event when the coordinator receives command as shown in the star in the figure.
The coordinator wants to receive this command like ZPS_EVENT_NWK_LEAVE_INDICATION .
Hi Seung Ho Kim,
As you know, the Zigbee IoT Gateway Control Bridge is reporting to the host all the status events, commands, etc.
So, if you look at app_ZncParser_task.c, APP_taskZncb, the Jenos task is processing the stack events.
case E_RUNNING:
.
.
.
if (sStackEvent.eType == ZPS_EVENT_NWK_LEAVE_INDICATION) {
.
.
.
Or you can display the event before the state consumes.
vDisplayStackEvent. app_zbp_utilities.c
Hope it helps.
Mario
Hi Seung Ho,
The coordinator is waiting for the leave command from the router. is this command that you are asking?
Or the router is leaving the network?
Are The Router and ED working with our application notes?
Mario