Wakeup PN7462 on falling edge of GPIO interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wakeup PN7462 on falling edge of GPIO interrupt

979 Views
Bhavin_Dhulkotiya
Contributor II

Hi,

In our custom board, we are using PN7462 IC. We are putting PN7462 into standby mode. We want to wake up on the falling edge of GPIO interrupt. We have tried with the below example code.

After further debugging we come across section 8.3.4 Wake-up from Standby/Suspend Mode in the datasheet we found PN7462 wakes up on GPIO transition 0 to 1 (Rising edge). How to wake up on GPIO transition 1 to 0 (Falling edge) as our costume board required to use falling edge?

clipboard-image.png

0 Kudos
1 Reply

924 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @Bhavin_Dhulkotiya ,

 

I have checked with the expert team, and it seems that GPIO wakeup only supports 0 to 1.

 

Sorry for the inconvenience that has caused.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------