Hi Support,
Can I have the application note AN12849?
As title, I would like to know how to wake up host using Bluetooth.
If any information can be shared, it will be helpful.
Thanks.
Hello,
I apologize for the inconvenience this might cause you ,could you please help me with more details on where you got the information and the image you published? I had to remove it as this is a public space and the image contained confidential information where an NDA is needed. By any chance, do you have a sales representative or a direct NXP contact ?
You could try requesting the files as well , when looking into the part number you desire, you will need to go to the documentation section, go to the secure files option and request higher access where you will be shown some options there for you to request the file
Regards
Hi Support,
Actually, I only had the contact window of Azurewave rather than NXP.
I've been informed that this document might be helpful but I can't get this document from Azurewave due to confidential reason. That's why I have this request here directly.
Would it be possible that you can send this document to me directly through the mail?
My question is that I want to know how to wake up host using Bluetooth with module AW-CM276MA-PUR.
If you have the SOP document, it would be the best.
BTW, one more question, may I know the Bluetooth power consumption of AW-CM276MA-PUR when the host is in sleep mode? Do you have such information?
Thank you in advance.
hello,
I apologize but I can't provide the document directly through email, this should be downloaded by every customer due to the same confidentiality reasons, still , you can request the file directly.
Could you please help me enter the NXP web page and sign into your account ?
After being sure that you started your session could you please enter the part web page ?
Then you will go to the Design Resources section in the Documentation tab, after getting there , you should select the Secure Files option
Once you select that option , you should be able to see more files available there . Could you please help me confirm if you have some files available there ?
If you do not get to see any , there is a button for request higher access , could you please help me trying requesting higher access?
Also, for the power consumption, while we have some data related to the IC, if you are looking for the module consumption you should go with the module manufacturer . I apologize for the inconvenience this might cause you.
Regards,
Hi Support,
Thank you for the information.
However, I can't see the same options like you. Please check my screenshot below.
Could you please guide me how should I see that "Secure Files" option?
Whether I have the sufficient priviledge?
Thanks.
Hello,
No problem .
1.- First you will need to be logged into your account
2.- Once you are in your account , you will need to go to the web page of the device in this link.
3.- You will need to go to the documentation
4.- After that , you will get the same view as I have
Regards
Hello!
I am also interested in learning how to set up the wakeup functionality of the AW-CM276MA-PUR module. I have been granted with access following your instructions, but I don't see any document in the "Secure Files" section. Could you please indicate if any other step is needed? Or where to find the information for the wakeup functionality AW-CM276MA-PUR module.
Thanks!
BR