Update OTA fail !

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update OTA fail !

959 Views
minhtan_uet
Contributor III

Hi Support team :smileygrin:

Relate to:
how to add a point in jn-an-1218-zigbee-3-0-light-bulb 
return E_ZCL_FAIL when register endpoint 
Now I'm working with JN-AN-1218-Zigbee-3-0-Light-Bulb. But I get a ploblem.
When I update OTA to DimmableLight note have 1 endpoint , It work well
Then I haved added another Endpoint, It work well with normal firmware. The problem occurred when I uploaded the OTA firmware. Router can't join to network

pastedImage_4.png

Can you help me !!! Thanks

Labels (1)
0 Kudos
3 Replies

792 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Tran Minh Tan, I hope you're doing well!

 

Just to clarify, did you change the build configuration to enable generation for new OTA files?

 pastedImage_1.png

 

Could you please verify if new OTA files are being generated during the compiling process?

 

Please let me know of your findings.

 

Best regards,

Sebastian

0 Kudos

792 Views
minhtan_uet
Contributor III

Dear Sebastian Delrio Employee
Thank for reply :smileygrin:
I have try. But it still get crash and reset.

pastedImage_1.png

pastedImage_3.png
Thanks

0 Kudos

792 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Tran Minh Tan,

 

If I'm understanding correctly, you programmed your device with the full OTA binary with only one End Point, then you sent the OTA upgrade with two End Points, and when the device reset, it crashed, correct?

 

Does the device also crash if you program the OTA binary directly instead of sending the .ota file to it?

 

pastedImage_1.png

 

Best regards,

Sebastian

0 Kudos