Unable to open probe index 1. Error: Probe not open

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to open probe index 1. Error: Probe not open

Jump to solution
2,154 Views
frank-li2021
Contributor III

I'm using micro-usb for power supply and openSDA to debug the KW36 board

IDE mcuXpresso can probe the cmsis-dap, but show err msg as below

 

frankli2021_0-1632712276716.pngfrankli2021_1-1632712282151.pngfrankli2021_2-1632712286949.png

 

And each time I have the problem, reboot pc w'll be ok in new debug session

0 Kudos
1 Solution
2,093 Views
nxf56274
NXP Employee
NXP Employee

debug固件的问题,简单说,有不同的调试固件包括cmsis-dap,jlink,等等dap固件不行,于是就换成jlink固件

View solution in original post

13 Replies
2,142 Views
kerryzhou
NXP TechSupport
NXP TechSupport

@nxf56274,

   Hello Da Li, please help the customer check the KW36 issues, thanks.

 

0 Kudos
2,152 Views
frank-li2021
Contributor III
0 Kudos
2,128 Views
nxf56274
NXP Employee
NXP Employee

把debug固件改成jlink。长按复位按钮,然后插usb,磁盘应该出现一个类似daplinkboot的盘符,然后把附件解压,把bin文件拖进去,然后再试试

2,117 Views
frank-li2021
Contributor III

感谢回复,如何设置 jlink,需要 jlink 工具接 pc 吗

0 Kudos
2,112 Views
nxf56274
NXP Employee
NXP Employee

按上面说的更新完固件就行了,不需要设置什么,然后mcuxpresso按住shift+debug来重新调试

0 Kudos
2,109 Views
frank-li2021
Contributor III

shift+debug 是什么意思?

0 Kudos
2,103 Views
nxf56274
NXP Employee
NXP Employee

键盘的shift,mcuxpesso的debug选项

2,101 Views
frank-li2021
Contributor III

嗯 force probe 确实可以了,但是之前可以识别到 CMSIS-DAP,

更新固件,shift + probe 之后,方式 变成了 jlink,这个对吗。效果确实是可以 debug 了,停在了 main

0 Kudos
2,098 Views
nxf56274
NXP Employee
NXP Employee

对的

0 Kudos
2,096 Views
frank-li2021
Contributor III

有点蒙圈了。。这个是为什么啊,能简单解释一下吗多谢啦

0 Kudos
2,094 Views
nxf56274
NXP Employee
NXP Employee

debug固件的问题,简单说,有不同的调试固件包括cmsis-dap,jlink,等等dap固件不行,于是就换成jlink固件

2,104 Views
frank-li2021
Contributor III

多谢知道了,shift+debug = force probe

0 Kudos
2,110 Views
frank-li2021
Contributor III

frankli2021_0-1632733092303.png

 

0 Kudos