我导入低功耗终端设备示例(FRDM-KW41Z),并将THREAD_USE_SHELL更改为1,这是文件./source/config.h中的宏定义。然后,我输入命令'thr join'到shell,但它打印'join failed'。
当我使用ED示例时,我成功加入。
因此,我用嗅探器观察。我发现两个例子的加入请求已经达成一致并且交换了密钥。
为什么?
Hello,
Which release and IDE are you using? Did you make any other change in the example?
By any chance, could you please reply in English?
Regards,
Estephania
I use MCUXpresso IDE v10.1.1_606 and import the example(thread_low_power_end_device).
I changed the macro definition THREAD_USE_SHELL in the file config.h to 1.
Then I type the command ‘thr join’ in the shell, but it prints out ‘join failed’.
I uploaded two sniffing messages, one was successfully added and the other was added by the example.
Based on shell log ( Thread version - 1.1.1.18), seems to be the same problem with the one from this topic : Thread low power end device examples can't thr join?
A new release including the fix for low power devices will be available at the end of July.
Regards,
Ovidiu