Hello,
I am trying to get the thread host interface example working.
I have downloaded the SDK from Welcome to MCUXpresso | MCUXpresso Config Tools and I am trying to run the frdmkw41z_wireless_examples_thread_host_controlled_device_freertos example.
I have flashed it to my frdmkw41z board, which flashes the RGB LED blue. I connected a UART to USB adapter running on COM 4.
I downloaded the NXP Test Tool 12 to test out the THCI functionality. It recognizes the com port. Whenever I send a command, there is a TX entry but no RX response. If I plug the board in when its off, I can see a few RX commands as the board starts up.
Any help would be greatly appreciated.
Hello,
To try to recreate your issue, could you please tell me which IDE are you using?
Best Regards,
Estephania
Hello,
I am using the MCUXpresso IDE v10.0.2 [Build 411] [2017-07-11] .
Thank you in advance!
Piers
Hello,
I used the latest version available in the MCUXpresso web page, and I did not have any problem while working with the Test Tool.
Which baud rate are you using?
Best Regards,
Estephania