Thread Example Not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Thread Example Not working

708 Views
pierslfx
Contributor I

Hello,

I am trying to get the thread host interface example working.

I have downloaded the SDK from Welcome to MCUXpresso | MCUXpresso Config Tools  and I am trying to run the frdmkw41z_wireless_examples_thread_host_controlled_device_freertos example. 

I have flashed it to my frdmkw41z board, which flashes the RGB LED blue. I connected a UART to USB adapter running on COM 4.

I downloaded the NXP Test Tool 12 to test out the THCI functionality. It recognizes the com port. Whenever I send a command, there is a TX entry but no RX response. If I plug the board in when its off, I can see a few RX commands as the board starts up.

Any help would be greatly appreciated.

0 Kudos
3 Replies

532 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

To try to recreate your issue, could you please tell me which IDE are you using?

Best Regards,

Estephania  

0 Kudos

532 Views
pierslfx
Contributor I

Hello,

I am using the MCUXpresso IDE v10.0.2 [Build 411] [2017-07-11] .

Thank you in advance!

Piers

0 Kudos

532 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

I used the latest version available in the MCUXpresso web page, and I did not have any problem while working with the Test Tool. 

THR_hcd.PNG

Which baud rate are you using? 

Best Regards, 

Estephania 

0 Kudos