The main (handheld) and anchor points (sub-anchor points and main anchor points) of KW38.
Now what we need is for handheld device A to be able to connect to anchor point A. Now let's say that anchor point A is disconnected from handheld device A, and handheld device A can connect to anchor point B.
If I want to implement such a feature, what should I do?I did this by placing the anchor IRK in handheld device A.This is when handheld device A scans to anchor point A or anchor point B, which is connected to anchor point A or anchor point B.
But this is not the case.Handheld device A is just connected to the anchor IRK that holds the first location.
What can I do so that I can hold A (the IRK that holds anchor A and anchor B) and connect to anchor A or anchor B?
Tell me, guide me, thank you!
Hello,
I sent you a private message.
Regards,
Ricardo