The best way to build a PCB using a KW45 (car access) or K32W1 (IoT/Industrial) first time right

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The best way to build a PCB using a KW45 (car access) or K32W1 (IoT/Industrial) first time right

4,242 Views
christophe_menard
NXP Employee
NXP Employee

Please, find the important link to build a PCB using a KW45 or K32W1 and all concerning the radio performances, low power and radio certification (CE/FCC/IC).

 

KW45 product NXP web page:

https://www.nxp.com/products/wireless/bluetooth-low-energy/32-bit-bluetooth-5-3-long-range-mcus-with...

 

K32W1 product NXP web page:

https://www.nxp.com/products/wireless/multiprotocol-mcus/tri-core-secure-and-ultra-low-power-mcu-for...

 

KW45-EVK getting started NXP web page

https://www.nxp.com/products/processors-and-microcontrollers/kw45b41z-evaluation-kit-with-bluetooth-...

https://www.nxp.com/document/guide/getting-started-with-the-kw45b41z-evaluation-kit:GS-KW45B41ZEVK

K32W1-EVK getting started NXP web page

https://www.nxp.com/products/processors-and-microcontrollers/k32w148-evaluation-kit-with-multiprotoc...

https://www.nxp.com/document/guide/getting-started-with-the-k32w148-development-platform:GS-K32W148E...

 

HW:

    KW45-EVK HW guideline: Hardware Design Considerations for KW45B41Z and K32W148 Bluetooth LE Devices (nxp.com)

    KW45B41Z-EVK User Manual https://www.nxp.com/docs/en/user-manual/KW45B41Z-EVKUM.pdf

    K32W1-EVK User Manual

    Minimum BoM (attached file)

    DCDC management guide (AN13831) : KW45/K32W148 - Power Management Hardware (nxp.com)

    Migration guide: KW38 to KW45: coming soon

    Design-In check list: excel file attached

    RF matching: S parameters (file provided by request)

 

Radio:

    RF report: KW45 and K32W148 RF System Evaluation Report for Bluetooth LE and K32W148 for 802.15.4 Applications ...

    Radio co-existance: Kinetis Wireless Family Products Bluetooth Low Energy Coexistence with Wi-Fi Application (nxp.com)

    Low Power Consumption: https://www.nxp.com/docs/en/application-note/AN13230.pdf

    Distance performances: refer to attached file

    Antenna: https://www.nxp.com/docs/en/application-note/AN2731.pdf

    Generic FSK Link Layer Quick Start (attached file)

    BLE connectectivity test binary file:  SDK_x_xx_x_KW45B41Z-EVK\boards\kw45b41zevk\wireless_examples\genfsk\connectivity_test\bm\iar\

    K32W148 Connectivity Test for 802.15.4 Application (nxp.com)

    Return loss (S11) measurement: How to measure the return loss of your RF matching (S11)

                   part of the RF report (AN13728)

    Loadpull: Kinetis KW45 and K32W148 Loadpull Report (nxp.com)

SW tools:

    IoT Tool box (mobile application)

    Connectivity test tool for connectivity products (part of the IoT toolbox)

    DTM: How to use the HCI_bb on Kinetis family products a... - NXP Community

https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/BLE-HCI-Application-to-set-transmitter-...

 

Crystal

Article 1 : KW45/K32W1 32MHz & 32kHz Oscilllation margins - NXP Community

Article 2 : KW45/K32W1 32MHz & 32kHz Oscilllation margins

KW36 - Trimming adjust of 32MHz XTAL external osci... - NXP Community

 

LowPower Estimator Tool

Excel attached file

 

Certification:

EUROPEAN UNION (nxp.com)

7 Replies

969 Views
xing_chang
NXP Employee
NXP Employee

Hi @christophe_menard ,

In the checklist, we should add a check on the external watchdog, note that if the customer uses the OTA function, when upgrading the firmware, the time required after reset may reach a few seconds, which requires special attention from the external watchdog.

0 Kudos

1,519 Views
suleymansekerci
Contributor I

Does anyone help me to about the value of power consumption for KW54 in three modes( PMIC, DCDC, Bypass) ?

0 Kudos

1,485 Views
christophe_menard
NXP Employee
NXP Employee

Hi Suleymansekerci,

Could you precise your request about the three modes( PMIC, DCDC, Bypass), please?

For your help, you could refer to the AN13230 Kinetis KW45 & K32W1 Bluetooth LE Power Consumption Analysis available in NXP site and playing with the KW45_BLE_power_profile_calculator_v1.5.xlsx file.

 

For your guidance, the most safe power is the buck mode (DCDC inside the Kinetis product)  for sure without any extra BoM cost. 

1,467 Views
suleymansekerci
Contributor I

Dear Menard,

 

Thanks  for your reply.

 

BR

0 Kudos

3,752 Views
christophe_menard
NXP Employee
NXP Employee

Hi Marko,

The added components are not the same on the 3 use cases.

0 Kudos

3,755 Views
christophe_menard
NXP Employee
NXP Employee

Hi Marko,

The valus are correct. The added components are not the same on the 3 use cases.

0 Kudos

3,763 Views
marko_pavlin
Contributor I

Hi, I am looking the "minimum BOM" document. At the end, there is a table with con-cell operation recommendation:

marko_pavlin_1-1680760460835.png

Is this OK? 10dBm <1mA, ... 0dBm : 4,5mA ?

 

0 Kudos