Please, find the important link to build a PCB using a KW45 or K32W1 and all concerning the radio performances, low power and radio certification (CE/FCC/IC).
KW45 product NXP web page:
K32W1 product NXP web page:
KW45-EVK getting started NXP web page
https://www.nxp.com/document/guide/getting-started-with-the-kw45b41z-evaluation-kit:GS-KW45B41ZEVK
K32W1-EVK getting started NXP web page
HW:
KW45-EVK HW guideline: Hardware Design Considerations for KW45B41Z and K32W148 Bluetooth LE Devices (nxp.com)
KW45B41Z-EVK User Manual https://www.nxp.com/docs/en/user-manual/KW45B41Z-EVKUM.pdf
K32W1-EVK User Manual
Minimum BoM (attached file)
DCDC management guide (AN13831) : KW45/K32W148 - Power Management Hardware (nxp.com)
Migration guide: KW38 to KW45: coming soon
Design-In check list: excel file attached
RF matching: S parameters (file provided by request)
Information: “As RF behavior are dependent of PCB layout & manufacturing; PCB prototypes (based on NXP recommendations) will have to be fine-tuned to insure the expected qualified in RF is reached on the final productized platform.”
Radio:
Radio co-existance: Kinetis Wireless Family Products Bluetooth Low Energy Coexistence with Wi-Fi Application (nxp.com)
Low Power Consumption: https://www.nxp.com/docs/en/application-note/AN13230.pdf
Distance performances: refer to attached file
Antenna: https://www.nxp.com/docs/en/application-note/AN2731.pdf
Generic FSK Link Layer Quick Start (attached file)
BLE connectectivity test binary file: SDK_x_xx_x_KW45B41Z-EVK\boards\kw45b41zevk\wireless_examples\genfsk\connectivity_test\bm\iar\
K32W148 Connectivity Test for 802.15.4 Application (nxp.com)
Return loss (S11) measurement: How to measure the return loss of your RF matching (S11)
part of the RF report (AN13728)
Loadpull: Kinetis KW45 and K32W148 Loadpull Report (nxp.com)
SW tools:
IoT Tool box (mobile application)
Connectivity test tool for connectivity products (part of the IoT toolbox)
DTM: How to use the HCI_bb on Kinetis family products a... - NXP Community
Crystal
Article 1 : KW45/K32W1 32MHz & 32kHz Oscilllation margins - NXP Community
Article 2 : KW45/K32W1 32MHz & 32kHz Oscilllation margins
KW36 - Trimming adjust of 32MHz XTAL external osci... - NXP Community
LowPower Estimator Tool
Certification:
Hi @christophe_menard ,
In the checklist, we should add a check on the external watchdog, note that if the customer uses the OTA function, when upgrading the firmware, the time required after reset may reach a few seconds, which requires special attention from the external watchdog.
Does anyone help me to about the value of power consumption for KW54 in three modes( PMIC, DCDC, Bypass) ?
Hi Suleymansekerci,
Could you precise your request about the three modes( PMIC, DCDC, Bypass), please?
For your help, you could refer to the AN13230 Kinetis KW45 & K32W1 Bluetooth LE Power Consumption Analysis available in NXP site and playing with the KW45_BLE_power_profile_calculator_v1.5.xlsx file.
For your guidance, the most safe power is the buck mode (DCDC inside the Kinetis product) for sure without any extra BoM cost.
Dear Menard,
Thanks for your reply.
BR
Hi Marko,
The added components are not the same on the 3 use cases.
Hi Marko,
The valus are correct. The added components are not the same on the 3 use cases.
Hi, I am looking the "minimum BOM" document. At the end, there is a table with con-cell operation recommendation:
Is this OK? 10dBm <1mA, ... 0dBm : 4,5mA ?