Setting TX power level in BLE Host stack has no effect on peak current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting TX power level in BLE Host stack has no effect on peak current

Jump to solution
1,276 Views
arpad_toth
Contributor II

Hello,

Setting power level in "BLE Host stack QN9080DK MCUXpresso SDK 2.2.0" stack has NO effect on TX advertisement current level, with these two power level the peak current is still 0.9mA:

Gap_SetTxPowerLevel(0u, gTxPowerAdvChannel_c)
Gap_SetTxPowerLevel(255u, gTxPowerAdvChannel_c)

BleApp_GenericCallback(const gapGenericEvent_t* const pGenericEvent)
{
      switch(pGenericEvent->eventType)
      {
            case gInitializationComplete_c:
                  /* set TX power */
                  assert(Gap_SetTxPowerLevel(255u, gTxPowerAdvChannel_c) == gBleSuccess_c);
                  assert(Gap_SetTxPowerLevel(255u, gTxPowerConnChannel_c) == gBleSuccess_c);
                  break;
                  ...
            case gTxPowerLevelSetComplete_c:
                  /* this is called twice, break point stops here */
                  break;
}

Also RSSI on RX side doesn't seem to be correlating.

What am I doing wrong?

Labels (2)
Tags (3)
0 Kudos
1 Solution
1,015 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello ,

  The register that needs to be modified it's the ANA_CTRL0[PA_POWER], the  API to access this register is RF_SetTxPowerLevel(). It can be set between 0x00 (minimum -  -30dBm) and 0xFF (maximum - +2dBm). 

 

  By default this field is not touched, so it is set to 0x7F which corresponds to 0dBm. 

Regards,
Estephania

View solution in original post

0 Kudos
2 Replies
1,015 Views
arpad_toth
Contributor II

Controller_SetTxPowerLevel() is not an active interface for QN908X.

0 Kudos
1,016 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello ,

  The register that needs to be modified it's the ANA_CTRL0[PA_POWER], the  API to access this register is RF_SetTxPowerLevel(). It can be set between 0x00 (minimum -  -30dBm) and 0xFF (maximum - +2dBm). 

 

  By default this field is not touched, so it is set to 0x7F which corresponds to 0dBm. 

Regards,
Estephania

0 Kudos