SDK_2.2_QN908xCDK_Beta_Win_b170713.exe

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK_2.2_QN908xCDK_Beta_Win_b170713.exe

988 Views
seanwu
Contributor IV

Dear Sir,

I got an issue about QN908x beta SDK. I tried the BLE example like Wireless UART.

The BLE example will crash at NVDS_Init();

Could you please help me to ask what the problem is?

The other BLE examples which call NVDS_Init(); also have the same issue.

 

Thanks.

BR,

Sean

pastedImage_2.png

pastedImage_1.png

pastedImage_3.png

Labels (1)
Tags (4)
0 Kudos
6 Replies

625 Views
gerardo_rodriguez
NXP Employee
NXP Employee

Hello seanwu,

Just to confirm, are you using the latest version of MCUXpresso IDE v10.0.2?

What is the chip revision of your board? The MCUXpresso SDK for QN908x requires Rev C or later silicon.

Regards,

Gerardo

0 Kudos

625 Views
seanwu
Contributor IV

Dear sir,

I am using MCUXpresso IDE v10.0.2, and the EVB is QN9080 DK-V1.1.

The MCU is 9083, but I am not sure what the version is .

pastedImage_1.png

Thanks.

BR,

Sean

0 Kudos

625 Views
gerardo_rodriguez
NXP Employee
NXP Employee

Hi Sean,

According to the datasheet:

pastedImage_2.pngpastedImage_4.png

The WLCSP package has the following top-side marking:
• Line A: “9083”
• Line B1: xxxxxx

• Line B2: xxWW
   – WW: week code
• Line C: YY[R]x
   – YY: year code, 17 for 2017
   – R = Chip revision

Unfortunately, your chip revision is A, so the MCUXpresso SDK will be incompatible with your board.

Regards,

Gerardo

625 Views
anhvu
Contributor I

Dear sir,

unfortunately, I'm having a board with chip revision A, what can i do to test the BLE examples in the SDK?

BR

0 Kudos

625 Views
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Anh Vu,

Unfortunately, the latest SDK is not compatible with chip revision A. Sorry for the inconveniences.

Regards,

Gerardo

0 Kudos

625 Views
seanwu
Contributor IV

Dear sir,

Thanks your help.

BR,

Sean

0 Kudos