We want to run Cloud-Connected zigbee Demo and brought all the tower system boards its suggests:
Freescale Cloud-Connected ZigBee Thermostat Demo
I want to ask about the software we need to compile the software demo. According to demo user guide, are the following softwares needed?
1. IAR Embedded Workbench for ARM v7.10.1 (for K70 and Kw24zigbee)
2. CodeWarrior for MCUs v10.6. (for MC13237zigbee).
MQX RTOS v4.0.2
We program K70 use codewarrior before. Do we need to use IAR to run sw demo? Since we only have Codewarrior now, I wonder is the IAR neccery?
Any suggestions are very grateful. It would br better to list the software enviroment and version. Thank you so much!
Hi Dongyang,
You can use CodeWarrior for MCUs v10.6 to compile the MC13237 project but you will need IAR Embedded Workbench for ARM v7.10.1 for both the K70 and KW24 projects.
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer